7 Appendix 3: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under directory HW. If required, the design flow can be reproduced from the Design Implementation before the job file is generated.
To run the TCL, perform the following steps:
- Launch the Libero® software.
- Select
- Click Browse and from the downloaded
HWdirectory, selectscript.tcl - Click Run.
After successful execution of TCL script, Libero project is created within HW directory.
For more information about TCL scripts, see
mpf_an4660_df/HW/TCL_Scripts_readme.txt.
For more details on TCL commands, see Tcl Commands Reference Guide . Contact Technical Support for any queries encountered when running the TCL script.