9 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the current publication.

Table 9-1. Revision History
RevisionDateDescription
D05/2025Updated the TCL filepath in the Appendix 3: Running the TCL Script section
C04/2025The following is the list of changes in revision C of the document:
  • Updated the IAP design with the TCK frequency constraint in the SDC file
  • Updated the .job filepath throughout the document
B07/2024The following is the list of changes in revision B of the document:
A08/2022The following is the list of changes in revision A of the document:
7.0—Added Appendix 3: Running the TCL Script.
6.0— The following is a summary of the changes made in this revision.
  • Updated the document for Libero SoC v12.2
  • Removed the references to Libero version numbers
5.0—The document was updated for Libero SoC v12.0
4.0—Merged Splash kit related content and updated the document for Libero SoC PolarFire v2.3 release
3.0—The document was updated for Libero SoC PolarFire v2.2 release
2.0—The document was updated for Libero SoC PolarFire v2.1 release
1.0—The first publication of this document