2 Libero Design Flow
(Ask a Question)The Libero design flow involves running the following processes in the Libero SoC.
Important:
- To initialize the TCM in PolarFire using the System Controller, a local parameter
l_cfg_hard_tcm0_en, in themiv_rv32_subsys_pkg.vfile must be changed to 1’b1 prior to synthesis. For more information, see the 2.7 TCM section in the MIV_RV32 Handbook. This user guide can be downloaded from the Libero SoC Catalog. - In case any error is observed related
to address space access issue, ensure to perform this step: Navigate to , and then Enable "Downgrade memory map generation DRC
errors to warnings" as shown in the following figure.
Figure 2-1. Project Settings
The following figure shows these options in the Design Flow tab.