5.3.2.10 Set Beacon Data (IB/NB)
Format:
IB,<hex8>,<Hex>
NB,<hex8>,<Hex>
These commands are used for the beacon advertisement. For more details, refer to Set Extended Advertisement Data (IAE/NAE/ISE/NSE).
Using IB/NB will configure the second advertisement set to beacon with legacy advertising. The length of total data is limited to 31 bytes. It can have some advanced configurations by the IPE command if needed.
Note: The parameters of
NB commands are stored in PDS. The parameters are effective immediately after restarting the advertising without a reboot.