5.3.2.8 Set Deep Sleep Advertising (SDO,<0,1>,<hex16>)
Format: SDO,<0,1>,<hex16>
The Deep Sleep Advertising (DSADV) in the RNBD350 module is configurable using the SDO command. The SDO command accepts two input parameters. The first parameter is a single digit value that determines the enabling/disabling of the deep sleep advertising feature, and it expects two bytes length as the second input parameter. The value ‘1’ enables the deep sleep advertisement. When the deep sleep advertisement is enabled, then the UART is not operational to save the power consumption. If the first parameter value is ‘0’, the RNBD350 module runs without DSADV and UART is operational all time.
It is necessary to wake up UART by pulling UART_RX_IND (UART RX Indication, PB4) pin low from the host MCU before the host MCU transmits data to the RNBD350 module.
The second input parameter indicates the deep sleep advertisement interval with a 0.625 ms time unit.
With deep sleep advertisement enabled, the RNBD350 module wakes up and advertises once for every set interval time. After the single advertisement, the RNBD350 module enters into deep sleep again until it gets connected with a central.
If the DSADV interval setting is more than 400 ms, the RNBD350 module rejects DSADV. In this scenario, there is no power consumption advantage than normal Sleep mode, and the RNBD350 module rejects the DSADV. MCU can choose the normal Sleep mode command instead of the Low Power Control (SO) command. For more details, refer to Low Power Control (SO,<0,1>).
| Default: | 0, 0000 | // DSADV mode is disabled |
| Example: | SDO,1,0640 | // Set DSADV to enabled for interval 1s |
| Response: | AOK | // Success |
Err | // Syntax error or invalid parameter |