5.4.2.1 Set Firmware Version
Format: SDF,<text>
This command sets the value of the firmware revision characteristics in the device information service. This command is only effective if the device information service is enabled by command SS.
Use the device information service to identify the device. All its characteristics rarely change. Therefore, values of characteristics in the device information service are set and saved into PDS. All of the values of the characteristics in the device information service have a maximum size of 20 bytes.
For more information on the device information service, refer to the Bluetooth Core Specification.
| Item | Firmware Version 1.0 and Later | Description |
|---|---|---|
| Default: | Current RNBD350 firmware version | |
| Example: | SDF,0.9 | — |
| Response: | AOK | Success |
Err | Device information service not enabled Syntax error, invalid parameter | |
Note:
| ||