27.3.2.5 Synchronous Slave Reception Setup:
- Set the SYNC and SPEN bits and clear the CSRC bit.
- Select the receive input pin by writing the appropriate value to the RXxPPS register.
- Select the clock input pin by writing the appropriate values to the CKxPPS register.
- Clear the ANSEL bit for both the TXx/CKx and RXx/DTx pins (if applicable).
- If interrupts are desired, set the RCxIE bit of the PIEx register and the GIE and PEIE bits of the INTCON register.
- If 9-bit reception is desired, set the RX9 bit.
- Set the CREN bit to enable reception.
- The RCxIF bit will be set when reception is complete. An interrupt will be generated if the RCxIE bit was set.
- If 9-bit mode is enabled, retrieve the Most Significant bit from the RX9D bit of the RCxSTA register.
- Retrieve the eight Least Significant bits from the receive FIFO by reading the RCxREG register.
- If an overrun error occurs, clear the error by either clearing the CREN bit of the RCxSTA register or by clearing the SPEN bit which resets the EUSART.