4.2.2.3 MSS E51 Processor Watchdog Timeout Reset

The MSS can be configured such that the E51 processor’s watchdog timer causes a reset of the MSS when the timer runs out.

MSS Reset Reasons

MSS can be reset in various ways as explained in the preceding sections. The user can access the 32-bit register RESET_SR to know which reset caused the MSS to be reset. The following table lists the reasons for resetting the MSS.

Table 4-2. MSS Reset Reasons
ReasonReset Reason BitAsserted ByNotes
SCB_PERIPH_RESET0SCBThis is the power-on reset. This fully resets the MSS including eNVM trim values. Additional bits in the SOFT-RESET register also allow the SCB registers to be reset.
SCB_MSS_RESET1SCB, CPU, MSSThis resets the MSS including the Core Complex, Peripherals and all AXI infrastructure. It does not reset the eNVM trim values and SCB registers.
SCB_CPU_RESET2SCB, CPU, MSSThis resets the Core Complex only. This reset must not be used in most cases as the MSS requires resetting at the same time to clear outstanding AXI transactions and so on.
DEBUGGER_RESET3DebuggerThis is asserted by the Core Complex debugger and has the same effect as the SCB_MSS_RESET.
FABRIC_RESET4FabricThis signal is asserted by the fabric (MSS_RESET_N_F2M) and has the same effect as the SCB_MSS_RESET. This signal can be asserted at power-up to hold the MSS in reset. If not asserted at power-up, this signal can be used subsequently at any stage during normal operation to reset the MSS.
WDOG_RESET5WatchdogThis indicates that the watchdog reset has been activated.
GPIO_RESET6FabricThis indicates that the fabric asserts the MSS GPIO soft reset. This resets the GPIO blocks if the GPIOs are configured to be reset by this signal. This does not reset the MSS.
SCB_BUS_RESET7FabricIndicates that SCB bus reset has occurred.
CPU_SOFT_RESET8CPUIndicates that the CPU resets the MSS using the soft reset register.
Reserved31:9—Reserved

It is normal for multiple bits of RESET_SR to be enabled, as most of them are interconnected from a hardware perspective. For more information about RESET_SR, see the PolarFire SoC Register Map.