8.5.11 CONFIG11
Name: | CONFIG11 |
Offset: | 30 000Ah |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
BOOTPOR | COE | CFGSCEN | DATSCEN | SAFSCEN | APPSCEN | BOOTCOE | BOOTSCEN | ||
Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
Reset | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
Bit 7 – BOOTPOR CRC-on-Boot Enable
Value | Description |
---|---|
1 | CRC-on-boot disabled, device will immediately execute user code upon device Reset |
0 | CRC-on-boot enabled, device will perform CRC check of configured memory before executing user code upon device Reset |
Bit 6 – COE Continue on Error for Non-Boot Block Areas Enable
Value | Description |
---|---|
1 | Device will halt if a mismatch is found between expected and calculated CRC values for the non-boot block areas of memory |
0 | Device will continue execution even if a mismatch is found between expected and calculated CRC values for the non-boot block areas of memory |
Bit 5 – CFGSCEN Non-Boot Block Area CRC Configuration Fuse Scan Enable
Value | Description |
---|---|
1 | Non-boot block area CRC scan/calculation will not include Configuration Fuse values in its calculation |
0 | Non-boot block area CRC scan/calculation will include all Configuration Fuse values except CONFIG14H-CONFIG16L in its calculation |
Bit 4 – DATSCEN Non-Boot Block Area CRC Data EEPROM Scan Enable
Value | Description |
---|---|
1 | Non-boot block area CRC scan/calculation will not include Data EEPROM values in its calculation |
0 | Non-boot block area CRC scan/calculation will include Data EEPROM values in its calculation |
Bit 3 – SAFSCEN Non-Boot Block Area CRC SAF Area Scan Enable
Value | Description |
---|---|
1 | Non-boot block area CRC scan/calculation will not include SAF area of Flash memory in its calculation if SAF area is enabled |
0 | Non-boot block area CRC scan/calculation will include SAF area of Flash memory in its calculation if SAF area is enabled |
Bit 2 – APPSCEN Non-Boot Block Area CRC Application Code Area Scan Enable
Value | Description |
---|---|
1 | Non-boot block area CRC scan/calculation will not include main application code area of Flash memory in its calculations |
0 | Non-boot block area CRC scan/calculation will include main application code area of Flash memory in its calculations |
Bit 1 – BOOTCOE Continue on Error for Boot Block Areas Enable
Value | Description |
---|---|
1 | Device will halt if a mismatch is found between expected and calculated CRC values for the boot block areas of memory |
0 | Device will continue execution even if a mismatch is found between expected and calculated CRC values for the boot block areas of memory |
Bit 0 – BOOTSCEN Boot Block Area CRC Scan Enable
Value | Description |
---|---|
1 | CRC Scan/calculation on boot block area will not be run |
0 | CRC Scan/calculation on boot block area will be run |