Since the DV Run Time is not default content, it may be missing from Device Resources.
The image below shows how this is fixed for the Data Streamer, but the same process can
be followed for making the DV Run Time library available.
In this case click the button to open the MCC Content Manager.
CAUTION: Note that the MCC
Content Manager Icon, next to the icon is to
open the standalone version of the MCC Content Manger, i.e., where one can see all MCC
content. If attempting to open this, when MCC is running, the below message will be
triggered:
7.2 Builder: Add DV Run Time Library
Application Builder: Click 'Add Component'.
Filter on 'Data' then click the icon to add the DV Run Time.
Tip: When added to the Builder, components can be
considered to be in their default configuration.
CAUTION: If not in its default configuration, a Driver
or Library component's configuration can be reset by removing the component and
adding it back again.
Once added, the DV Run Time will be added to the MCC Builder.
Tip: Clicking the UART (None) or Timer (None) will
respectively bring the UART or Timer Driver to focus, from where a dependency can be
selected.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.