3 I2C Host Configuration
3.1 Builder: Add I2C Host Component
- Application Builder: Click 'Add Component'.
- Filter on 'I2C Host' then click the
icon to add the I2C_Host Driver.
Tip: There are a number of I2C off-chip drivers, such as I2C EEPROM AT24CM02 and I2C Temp Sensor MCP98xx, providing more specific support for these client devices.Tip: The I2C Host Example shows up as a loaded module, since it is already added to the project.
3.2 Builder: Select I2C PLIB
- Next, click Add Dependency to
select.
Tip: For AVR, the Two Wire Interface (TWIx) implements the I2C protocol.
CAUTION: If already added to the project, the
I2C PLIB may not be in its default configuration. A component's
configuration can be reset as follows:
- Click Register Initialization.
- From Track Changes, click
'Reset to MCC defaults'.
- Confirm that all user
changes will be reset.
3.3 Set I2Cx_Host Custom Name to I2C_Host
- Click the Custom Name field and
remove any numbering from the Peripheral Library (PLIB), setting the value to
I2C_Host.
Tip: Setting the Custom Name to a known value will set the name of the i2c_host_interface_t structure. It ensures that the generated example code will match that in the example. See below the code completion from MPLAB® X IDE.