7.6.24 Read Temperature Value
Description
The SPI command “Read Temperature Value” returns the temperature value of the latest measurement, which is stored in calib.sramTEMPH and calib.sramTEMPL.
Command Frame
| Host |
0x19 |
0x00 |
0x00 |
0x00 |
| ATA8510/15 |
events.system |
events.events |
tempVal_high |
tempVal_low |
Parameters
- 0x19 – Command ID
- 0x00 – Dummy byte (no information)
- 0x00 – Dummy byte (no information)
- 0x00 – Dummy byte (no information)
Return Values
- events.system – Event byte (for details see SPI command “Get Event Bytes”)
- events.events – Event byte (for details see SPI command “Get Event Bytes”)
- tempVal_high – calib.sramTEMPH
- tempVal_low – calib.sramTEMPL
The interpretation of the return values is not content of this document. The customer shall read the temperature value via the SPI command “Read SRAM / Register” from the SRAM variable calib.tempMeas as described in Temperature Measurement.