6.4.3 MAC Receive Block
All processing within the MAC receive block is implemented using a 16-bit data path. The MAC receive block checks for valid preamble, FCS, alignment and length, presents received frames to the FIFO interface and stores the frame destination address for use by the address checking block.
If, during the frame reception, the frame is found to be too long, a bad frame indication is sent to the FIFO interface. The receiver logic ceases to send data to memory as soon as this condition occurs.
At end of frame reception the receive block indicates to the DMA block whether the frame is good or bad. The DMA block will recover the current receive buffer if the frame was bad and the frame will not be forwarded to the SPI.
Ethernet frames are normally stored in DMA memory complete with the FCS. Setting the Remove FCS (RFCS) bit in the Network Configuration register causes frames to be stored without their corresponding FCS bytes. The reported frame length field is reduced by four bytes to reflect this operation.
The receive block signals to the statistics register block to increment the alignment, Frame Check Sequence Errors (FCSE), Undersize Frames Received (UFRX), Oversize Frames Received (OFRX), or Receive Symbol Errors (RXSE) when any of these exception conditions occur. A count of jabber errors received may be found within the integrated PHY status registers.
If the Ignore RX FCS (IRXFCS) bit is set in the Network Configuration register, CRC errors will be ignored and CRC errored frames will not be discarded, though the Frame Check Sequence Errors statistic register will still be incremented. This is useful for applications where individual frames with FCS errors must be identified.
Received frames can be checked for length field errors by setting the Length Field Error Frame Discard (LFERD) bit of the Network Configuration register. When this bit is set, the receiver compares a frame's measured length with the length field (bytes 13 and 14) extracted from the frame. The frame is discarded if the measured length is shorter. This checking procedure is for received frames between 64 bytes and 1518 bytes in length.
Each discarded frame is counted in the 8-bit Length Field Error (LFER) field of the statistics register. Frames where the length field is greater than or equal to 1536 will not be checked.