6.4.6 Hash Addressing
The hash address register is 64 bits long and takes up two locations in the memory map. The least significant bits are stored in Hash Register Bottom (MAC__HRB) and the most significant bits in Hash Register Top (MAC__HRT).
The Unicast Hash Enable (UNIHEN) and the Multicast Hash Enable (MTIHEN) bits in the Network Configuration register enable the reception of hash matched frames. The destination address is reduced to a 6-bit index into the 64-bit Hash register using the following hash function: The hash function is an exclusive OR (XOR) of every sixth bit of the destination address.
hash_index[05] = da[05] ^ da[11] ^ da[17] ^ da[23] ^ da[29] ^ da[35] ^ da[41] ^ da[47]
hash_index[04] = da[04] ^ da[10] ^ da[16] ^ da[22] ^ da[28] ^ da[34] ^ da[40] ^ da[46]
hash_index[03] = da[03] ^ da[09] ^ da[15] ^ da[21] ^ da[27] ^ da[33] ^ da[39] ^ da[45]
hash_index[02] = da[02] ^ da[08] ^ da[14] ^ da[20] ^ da[26] ^ da[32] ^ da[38] ^ da[44]
hash_index[01] = da[01] ^ da[07] ^ da[13] ^ da[19] ^ da[25] ^ da[31] ^ da[37] ^ da[43]
hash_index[00] = da[00] ^ da[06] ^ da[12] ^ da[18] ^ da[24] ^ da[30] ^ da[36] ^ da[42]
da[0] represents the
least significant bit of the first byte received, that is, the multicast/unicast
indicator, and da[47] represents the most significant bit of the last
byte received.
If the hash index points to a bit that is set in the Hash register then the frame will be matched according to whether the frame is multicast or unicast.
A multicast match will be signaled if
the multicast hash enable bit is set, da[0] is logic 1 and the hash
index points to a bit set in the Hash register.
A unicast match will be signaled if the
unicast hash enable bit is set, da[0] is logic 0 and the hash index
points to a bit set in the Hash register.
To receive all multicast frames, the Hash register should be set with all ones and the Multicast Hash Enable bit should be set in the Network Configuration register.