RAM Configuration
(Ask a Question)The following table lists the RAM configuration.
| RAM Configuration | Description |
|---|---|
| Write Port Depth | As specified in the RAM core generator dialog box (not editable). |
| Write Port Width | As specified in the RAM core generator dialog box (not editable). |
| Read Port Depth | As specified in the RAM core generator dialog box (not editable). |
| Read Port Width | As specified in the RAM core generator dialog box (not editable). |