3.3 Specifying Data in Memory File
(Ask a Question)If all the bits in the memory file are relevant, take steps to avoid bits from being ignored when the write port width is not aligned on a byte boundary. The following examples describe how to specify data in memory file so that the tool does not ignore bits. To avoid bits from being ignored, convert the hexadecimal data intended to initialize RAM into binary stream of bits, and then pad (insert) zeros based on the port width so that resulting data is byte-aligned, as described in the following sections.