2.2 Mutual Capacitance
Interaction between a mutual capacitance sensor and the human body is more complex. It may be modeled by considering two separate touch contacts to the X and Y electrodes, where each is capacitively coupled to the body, resistively connected to each other inside the body and capacitively coupled to earth via the human body capacitance.
A touch contact has two competing effects:
- The introduction of a conductive plate (finger) to both X and Y electrodes increases the capacitance between X and Y. This occurs if any conductive part is placed over the sensor.
- The addition of another capacitance (Ch + Cg) at the XY node provides an alternative path for the energy emitted by the X electrode, reducing the amount of charge accumulated on the sensor. This effect is manifested as an apparent reduction in the XY capacitance and occurs only if the body of material connected to the conductive part has a significant self-capacitance.
When a real touch contact is placed, the second (reducing) effect is much greater than the first (increasing) effect, and so a touch contact on a mutual capacitance sensor is indicated by an apparent reduction in sensor capacitance.