5.4.5 Module Reburst Flag
Module configuration and functionality are unique to each module, but any module may require a repeated measurement of specific sensors. To achieve this, a signal conditioning module may temporarily change the acquisition configuration, e.g., to disable those sensors not requiring reburst.
This is indicated to the application by the implementation of a common
‘Status’ byte at the first location of the signal conditioning group data
structure. A ‘1’ in bit 7 indicates that the application should
re-start measurement on the sensor group without waiting for the measurement cycle
time-out.
uint8_t qtm_xxx_status