3.3.2 Blue Bluetooth Status LED (D2)
The Blue Bluetooth Status LED (D2) indicates Bluetooth Low Energy connection status by specific LED Flash pattern.
Standby mode:
- No Bluetooth Low Energy connection
- RNBD451 is in Advertisement or Scan state
- Flash one time for every three seconds
- ON: 50 ms, OFF: 2950 ms
Linked mode:
- Bluetooth Low Energy ACL link is connected whether central or peripheral role
- Flash two times for every 1.5 seconds
- ON: 50 ms, OFF: 150 ms, ON: 50 ms, OFF: 1050 ms
Note: By default, the Bluetooth status LED is turned OFF. The user
can enable this feature by using the
SR command. For more details,
refer to the RNBD451 Bluetooth® Low Energy Module User’s
Guide (DS50003467).