Signal integrity issues on CA. When CMD/ADDR to REF_CLK training fails, a dialog box appears as
shown in the following figure.Figure 3-5. CMD/ADDR to REF_CLK
Training Fail
Workaround
Configure any one of the following parameters to a different value using the MSS Configurator when CMD/ADDR to REF_CLK (CA/CK) training fails:
Memory CA ODT
FPGA ADD/CMD Drive
The following figure shows the configuration of CA ODT in the DDR Memory Initialization tab.Figure 3-6. Configuring CA ODT—DDR Memory Initialization TabThe following figure shows the configuration of ADD/CMD drive in the DDR Controller tab.Figure 3-7. Configuring ADD/CMD Drive—DDR Controller Tab