3.1 ODT is not Turning ON
(Ask a Question)- Possible Reason
 - Signal integrity issue on CA. When the On Die Termination (ODT) does not turn ON, a dialog box
                    appears as shown in the following figure.
Figure 3-1. ODT is not Turning ON 
                     
- Workaround
 - Configure any one of the following parameters to a different value using the MSS Configurator when ODT does not turn ON:
 
- Additional Information
 - 
                    
If ODT is not ON and the remaining trainings pass, a dialog box appears as shown in the following figure.
Figure 3-4. ODT is not ON