Signal integrity issues on CA or DQS lines. When the Read Gate training fails, a dialog box
appears as shown in the following figure.Figure 3-11. Read Gate Training
Fail
Workaround
Configure any one of the following parameters to a different value using the MSS Configurator when the Read Gate training fails:
Memory CA ODT
Memory Pull-Down Drive Strength
FPGA DQS ODT
The following figure shows the configuration of pull-down drive strength or CA ODT in the DDR Memory Initialization tab.Figure 3-12. Configuring Pull-Down Drive Strength or CA ODT—DDR Memory Initialization TabThe following figure shows the configuration of DQS ODT in the DDR Controller tab.Figure 3-13. Configuring DQS ODT—DDR Controller Tab