4.3.1 Meaning of the Result Graphs in G3-PLC
The meaning of each result graph in the spreadsheets is described in the table below. The name of each one refers to the DUT operation, position and kind of data.
| Graph Name | Description |
|---|---|
| RSSI (dBµV) | The Received Signal Strength Indication in dBμV |
| Noised Symbols | Number of corrupted symbols in payload due to impulsive noise |
| Corrupted Carriers | Number of corrupted carriers in payload due to narrow/broad band noise |
| SNR BE (dB) | SNR of corrupted carriers in payload due to narrow/broad-band noise in quarters of dB |
| SNR Impulsive (dB) | SNR of corrupted symbols in payload due to impulsive noise in quarters of dB |
| SNR Background (dB) | Signal-to-Noise Ratio of the carriers that have not narrow band noise and from the symbols without impulsive noise |
| SNR Worst Carrier (dB) | Signal-to-Noise Ratio of the most noised carried in quarters of dB |
| SNR Worst Symbol (dB) | Signal-to-Noise Ratio of the most noised symbol in quarters of dB |
| SNR Header (dB) | The SNR Header is the SNR of the header in quarters of dB |
| SNR Payload (dB) | The SNR Payload is the SNR of the payload in quarters of dB |
| LQI (dB) |
The LQI parameter indicates the mean SNR per carrier. The LQI is an integer ranging from 0x00 to 0xFF and LQI values in-between are uniformly distributed between these two limits. The LQI value is derived from the average SNR (where averaging is done over all active tones and pilot tones, if present, in the bandplan and overall OFDM symbols in the received packet) where the SNR-to-LQI mapping is:
The value analyzed in the spreadsheet is the average of all LQI received. |
| FER (%) | Frame Error Rate, percentage of lost frames against sent frames. |
- A gain of 3 dB between the modulations BPSK, QPSK, 8PSK.
- Additional gain is obtained using ROBO modulation that adds more energy to each symbol.
- Sensitivity is improved with coherent modulations in exchange for greater complexity in the reception and lower baudrate.