4.3.2 Analysis of the Results in G3-PLC
Physical performance validation script results help to determine if a design is comparable with the Microchip reference designs. These tests allow detection of possible fails in the PLC reception or transmission paths associated with an incorrect PCB layout, incorrect component selection, etc.
Generally speaking, the most important result is the Frame Error Rate
that represents the number of frames with errors received in the function of the
attenuation (ATT) on the path or, more generally, depending on the received signal
strength indication (RSSI).
TX path results helps to determine:- Transmission Power: Depending on
the RSSI value obtained in the results, we can evaluate if the board is
transmitting the expected power. If the setup attenuation configuration is the
same, the RSSI of the received frames from DUT will be similar to the results
for the Microchip reference platform when the power supply source of the power
amplifier is the same (12V by default).
Figure 4-11. Typical RSSI Versus Attenuation on CEN_A with Microchip Reference EKs - On a clean environment setup, the TX path helps to analyze the transmission linearity of the DUT comparing the SNR_Payload, SNR Background or the LQI average for the same RSSI signal. Differences can be found mainly because of the transformer response on an isolated device but also there are no linear or ideal components, like coils, protection diodes or varistors, if no Microchip reference design BOM is selected.
- On a similar calibration and transmission path, the TX_RMSCALC values must be similar as on Microchip reference boards. Otherwise it is highly recommended to calibrate transmission parameters using Physical TX Calibration.
RX path results helps to determine:- Sensitivity: Depending on the FER
vs RSSI value obtained on the results, it can be determined if the background
noise of the DUT is lower to the limit to pass G3-PLC certification.Important: The G3-PLC certification Sensitivity Performance Test defines a maximum of 5% FER at 60 dBuV of RSSI when running the ROBO Differential modulation.According to the Microchip experience, on a typical meter device connected to AC mains:
Sensitivity (dBuV) RESULT <= 45 VERY GOOD 45 < TotalNoise <= 52 GOOD 52 < TotalNoise <= 58 POOR >58 POTENTIAL ISSUES - Impulsive Noise: Regarding Noised
Symbols, it can be determined if there is impulsive noise on the reception.
Additionally, comparing SNR Worst Symbol or SNR Impulsive with the SNR Payload,
its influence can be determined. It causes errors in symbols so, a frame can be
discarded depending on the impulsive intensity and the length of the frame
increasing the frame error rate.
Figure 4-12. Typical SNR Worst Symbol Versus RSSI on CEN_A Using DBPSK with Microchip Reference EKs Figure 4-13. Typical SNR Impulsive Versus RSSI on CEN_A Using DBPSK with Microchip Reference EKs Figure 4-14. Typical SNR Payload Versus RSSI on CEN_A Using DBPSK with Microchip Reference EKs - Narrowband Noise: Regarding
Corrupted Carriers, it can be determined if there is narrowband noise on the
reception. Additionally, comparing SNR Worst Carrier or SNR BE with the SNR
Payload, its influence can be determined. This kind of noise is continuous and
could be identified by accessing the SQLite database and analyzing the
RX_SNR_CARRIER result values for each frame sent. It could be identified too on
a clean environment when the G3-PLC Tone Map parameter does not correspond with
the expected. It can be analyzed with tools like Noise Test.
Figure 4-15. Typical SNR Worst Carrier Versus RSSI on CEN_A Using DBPSK with Microchip Reference EKs Figure 4-16. Typical SNR BE Versus RSSI on CEN_A Using DBPSK with Microchip Reference EKs - White Noise: If there is only
white Gaussian noise during the test, the
SNR payload, theSNR impulsive, theSNR beand theSNR backgroundare similar. It is not critical in terms of the reception (because it applies to the complete bandwidth) when the sensitivity limits are not reached and is usually due to thermal noise, wrong PC or component selection.Figure 4-17. Typical SNR Background Versus RSSI on CEN_A Using DBPSK with Microchip Reference EKs
- Continuous Narrow Band Noise: Usually associated with switching frequencies (or harmonics – mainly odd) of AC/DC and DC/DC converters. Follow Microchip PLC HW guidelines.
- Impulsive Noise: Usually associated with other asynchronous transfers like SPI, I2C, radiated coupling,commonly related to a poor PCB Layout or BOM. Follow Microchip PLC HW guidelines.
- Noise coming from mains.
| Modulation | Unit | CENELEC_A | CENELEC_B | ARIB | FCC |
|---|---|---|---|---|---|
| ROBO_D | dB | 1 | 1 | 2 | 1 |
| DBPSK | dB | 5 | 5 | 5 | 5 |
| DQPSK | dB | 8 | 8 | 8 | 8 |
| D8PSK | dB | 12 | 12 | 12 | 12 |
| ROBO_C | dB | 0 | 0 | 0 | 0 |
| BPSK_C | dB | 3 | 3 | 3 | 3 |
| QPSK_C | dB | 6 | 6 | 6 | 6 |
| 8PSK_C | dB | 10 | 10 | 10 | 10 |