Jump to main content
Introduction
1 Installing the Library
To use the libraries, install the MPLAB Code Configurator plug-in tool in the MPLAB X IDE. This section describes the installation of MCC and the Diagnostic Libraries.
2 Updating the Library
An update may be required if the library was previously installed and a new version is available. This section describes how to update the library using CMT in MCC.
3 Adding Diagnostic Tests
This section describes adding diagnostic tests using MCC Melody and the Diagnostic Libraries in MPLAB X projects.
4 Running the Examples
Examples are available for each diagnostic test. Users can generate these examples if the options are enabled in the user interface. For instance, to add the AVR SW_CPU_REGISTER_TEST_01 example:
5 Revision History