1.2.9.5 WDRV_PIC32MZW_PowerSaveListenIntervalSet Function
WDRV_PIC32MZW_STATUS WDRV_PIC32MZW_PowerSaveListenIntervalSet (
DRV_HANDLE handle, uint16_t u16ListenInt
);
C
Summary
Set the Wi-Fi listen interval for power save operation(in beacon period count).
Description
Set the Wi-Fi listen interval value for power save operation.It is given in units of Beacon period.
Periodically after the listen interval fires, the WiFi wakes up and listen to the beacon and check for any buffered frames for it from the AP.
A default value of 10 is used by the WiFi stack for listen interval. The user can override that value via this API.
Precondition
WDRV_PIC32MZW_Initialize should have been called. WDRV_PIC32MZW_Open should have been called to obtain a valid handle.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_PIC32MZW_Open. |
u16ListenInt | Listen interval in units of beacon period. |
Returns
WDRV_PIC32MZW_STATUS_OK - The request has been accepted. WDRV_PIC32MZW_STATUS_NOT_OPEN - The driver instance is not open. WDRV_PIC32MZW_STATUS_INVALID_ARG - The parameters were incorrect. WDRV_PIC32MZW_STATUS_REQUEST_ERROR - The request to the PIC32MZW was rejected.
Remarks
WDRV_PIC32MZW_PowerSaveListenIntervalSet should be called before WDRV_PIC32MZW_BSSConnect.