1.2.8.4 WDRV_PIC32MZW_APRekeyIntervalSet Function
WDRV_PIC32MZW_STATUS WDRV_PIC32MZW_APRekeyIntervalSet (
DRV_HANDLE handle, const uint32_t interval
)
C
Summary
Configures the group re-key interval used when operating in Soft-AP mode
Description
The re-key interval specifies how much time must elapse before a group re-key is initiated with connected stations. The timer is restarted after each group re-key.
Precondition
WDRV_PIC32MZW_Initialize should have been called. WDRV_PIC32MZW_Open should have been called to obtain a valid handle.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_PIC32MZW_Open. |
interval | The time in seconds that must pass before each re-key attempt. The minimum time value is 60 seconds. Defaults to 86400. |
Returns
WDRV_PIC32MZW_STATUS_OK - The request has been accepted. WDRV_PIC32MZW_STATUS_NOT_OPEN - The driver instance is not open. WDRV_PIC32MZW_STATUS_INVALID_ARG - The parameters were incorrect. WDRV_PIC32MZW_STATUS_REQUEST_ERROR - The request to the PIC32MZW was rejected.
Remarks
Takes effect after the next re-key - if an interval other than the default is desired then it is recommended to call this API before calling WDRV_PIC32MZW_APStart.