1.2.2.3 WDRV_PIC32MZW_Close Function
void WDRV_PIC32MZW_Close(DRV_HANDLE handle)
C
Summary
Closes an instance of the PIC32MZW driver.
Description
This is the function that closes an instance of the MAC. All per client data is released and the handle can no longer be used after this function is called.
Precondition
WDRV_PIC32MZW_Initialize should have been called. WDRV_PIC32MZW_Open should have been called to obtain a valid handle.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_PIC32MZW_Open. |
Returns
None.
Remarks
None.