Packing of Private Read Data by I3CC into Receive FIFO
The I3CC receives the bytes in the same order as on the bus and places the first byte received in the Least Significant Byte (LSB) position, and the following bytes in the LSB + 1 location, until all the four bytes of a word are received in the Receive FIFO. This is shown in the following figure.