Packing of Received ENTDAA data by I3CC into DCT Table.
The I3CC receives the bytes for the ENTDAA transfer in the same order as on the bus and places the first byte received in the Least Significant Byte position, and the following bytes in the LSB + 1 location, until all the four bytes of a word have been received in the DCT. The PID[47:16] is stored in the DCT base offset.
DCT_SECTION_OFFSET[TABLE_OFFSET] location and PID[15:0] are stored at DCT base offset + 1 location, BCR, DCR bytes at DCT base offset + 2 location, and assigned dynamic address in DCT base offset + 3 location. This is shown in the following figure.