3.3.133 UDDRC FREQ1 DFI Timing Register 1

Name: UDDRC_FREQ1_DFITMG1
Offset: 0x2194
Reset: 0x00000404
Property: Read/Write

Bit 3130292827262524 
       DFI_T_PARIN_LAT[1:0] 
Access R/WR/W 
Reset 00 
Bit 2322212019181716 
    DFI_T_WRDATA_DELAY[4:0] 
Access R/WR/WR/WR/WR/W 
Reset 00000 
Bit 15141312111098 
    DFI_T_DRAM_CLK_DISABLE[4:0] 
Access R/WR/WR/WR/WR/W 
Reset 00100 
Bit 76543210 
    DFI_T_DRAM_CLK_ENABLE[4:0] 
Access R/WR/WR/WR/WR/W 
Reset 00100 

Bits 25:24 – DFI_T_PARIN_LAT[1:0]

Specifies the number of DFI PHY clock cycles between when the dfi_cs signal is asserted and when the associated dfi_parity_in signal is driven.

Unit: DFI PHY clock cycles.

Programming Mode: Quasi-dynamic Group 4

Bits 20:16 – DFI_T_WRDATA_DELAY[4:0]

Specifies the number of DFI clock cycles between when the dfi_wrdata_en signal is asserted and when the corresponding write data transfer is completed on the DRAM bus.

This corresponds to the DFI timing parameter twrdata_delay. Refer to PHY specification for correct value.

For DFI 3.0 PHY, set to twrdata_delay, a new timing parameter introduced in DFI 3.0.

For DFI 2.1 PHY, set to tphy_wrdata + (delay of DFI write data to the DRAM).

Value to be programmed is in terms of DFI clocks, not PHY clocks.

In FREQ_RATIO=2, divide PHY's value by 2 and round up to next integer.

If using DFITMG0.dfi_wrdata_use_dfi_phy_clk=1, add 1 to the value.

Unit: DFI clock cycles.

Programming Mode: Quasi-dynamic Group 4

Bits 12:8 – DFI_T_DRAM_CLK_DISABLE[4:0]

Specifies the number of DFI clock cycles from the assertion of the dfi_dram_clk_disable signal on the DFI until the clock to the DRAM memory devices, at the PHY-DRAM boundary, maintains a low value. If the DFI clock and the memory clock are not phase aligned, this timing parameter should be rounded up to the next integer value.

Unit: DFI clock cycles.

Programming Mode: Quasi-dynamic Group 4

Bits 4:0 – DFI_T_DRAM_CLK_ENABLE[4:0]

Specifies the number of DFI clock cycles from the de-assertion of the dfi_dram_clk_disable signal on the DFI until the first valid rising edge of the clock to the DRAM memory devices, at the PHY-DRAM boundary. If the DFI clock and the memory clock are not phase aligned, this timing parameter should be rounded up to the next integer value.

Unit: DFI clock cycles.

Programming Mode: Quasi-dynamic Group 4