28.4.5 Advanced Features
Sleepwalking
SleepWalking is the capability for a device to temporarily wake up clocks for a peripheral to perform a task without waking up the CPU from Standby sleep mode. At the end of the sleepwalking task, the device can either be awakened by an interrupt (from a peripheral involved in SleepWalking) or enter again into Standby sleep mode.
In Standby when Sleepwalking is ongoing:
- All the power domains are turned ON including PDRAM power domain
- Low power mode of the regulators is not activated during sleepwalking
Wake-Up Time
As shown in the following figure, total wake-up time depends on:
- Latency due to Reference and Regulator effect.
- Latency due to Power Domain Gating:
Usually, wake-up time is measured with the assumption that the power domains are already in active state. When using Power Domain Gating, changing a power domain from OFF to active state will take a certain time, refer to Electrical Characteristics. If all power domains were already in active state in standby sleep mode, this latency is zero.
- Latency due to the CPU clock source wake-up time.
- Latency due to the NVM wake-up time from deep power down mode.