17.5.5 Debugger Security
The DSU provides Debug Access Level (DAL) mechanism which disable or limit the debugger access into the device. The DAL settings are programed through the ROMCFG.DAL fuse configuration bits.
The DSU DAL feature provides three levels of access. The following table describes the debugger access levels:
| DAL Setting | DSU Address Space | System Memory Regions (1) | Hot Plugging | Cold Plugging | ||
|---|---|---|---|---|---|---|
| External | Internal | Secure | Non-Secure | |||
| DAL 0 | X | - | - | - | - | X |
| DAL 1(1) | X | - | - | X | X | X |
| DAL 2 | X | X | X | X | X | X |
|
Note:
| ||||||
If the debugger attempts to access a device region which is not permitted by the current DAL setting, a bus error is returned to the CoreSight AP hardware which results in the assertion of the ARM DP sticky error bit.
In DAL0 mode, debugger breakpoints are disabled.