36.5.3.11 Management of OUT Pipes
OUT packets are sent by the host. All the data stored in the bank will be sent to the device provided the bank is filled. The pipe and its descriptor in RAM must be configured.
The host can send data to the device by writing to the data bank 0 in single bank or the data bank 0/1 in dual bank.
The generation of OUT packet starts when the pipe is unfrozen (PSTATUS.PFREEZE is zero).
The user writes the OUT data to the data buffer pointer by ADDR in the pipe descriptor and allows the USB to send the data by writing a one to the PSTATUS.BK0/1RDY. This will also cause a switch to the next bank if the OUT pipe is part of a dual bank configuration.
PINTFLAGn.TRCPT0/1 must be cleared before setting PSTATUS.BK0/1RDY to avoid missing an PINTFLAGn.TRCPT0/1 event.