8.2 Random Read
A random read begins in the same way as a byte write operation does
to load in a new data word address. This is known as a “dummy write” sequence; however, the
data byte and the Stop condition of the byte write must be omitted to prevent the part from
entering an internal write cycle. Once the device address and word address are clocked in
and acknowledged by the EEPROM, the bus host must generate another Start condition. The bus
host now initiates a current address read by sending a Start condition, followed by a valid
device address byte with the R/W bit set to
logic ‘1’. In this second device address byte for the AT24C04C and AT24C08C, the bit
positions usually reserved for the Most Significant bits of the word address (bit 1 for AT24C04C and bits 2 and 1 for AT24C08C) are "don't care" bits since the address that will be read from is
determined only by what was sent in the dummy write portion of the sequence. The EEPROM
will ACK the device address and serially clock out the data word on the SDA line. All types
of read operations will be terminated if the bus host does not respond with an ACK (it
NACKs) during the ninth clock cycle. After the NACK response, the host may send a Stop
condition to complete the protocol, or it can send a Start condition to begin the next
sequence.
- For the AT24C01C, AT24C02C and AT24C04C, the @ indicates the A1 hardware client address bit. For the AT24C08C, the @ indicates the A9 word address bit
(R/W =
0) or a “don't care” bit (R/W =1). - For the AT24C01C and AT24C02C, the $ indicates the A0
hardware client address bit. For the AT24C04C and AT24C08C, the $ indicates the A8 word address bit
(R/W =
0) or a “don't care” bit (R/W =1). - For the AT24C01C, the % indicates indicates a “don’t care” bit. For the AT24C02C, AT24C04C and AT24C08C, the % indicates the A7 word address bit.