1.5.4.3 AL_GetStatus Function

C

SYS_STATUS AL_GetStatus(void);

Summary

Gets the status of the AL module.

Description

This function allows to retrieve AL module status.

It must be used to ensure the module is Ready before start using it.

Parameters

None.

Returns

Returns the status of the Meters And Mores AL module.
  • SYS_STATUS_UNINITIALIZED: DLL module has not been initialized.
  • SYS_STATUS_READY: DLL module is ready to be used.

Example

    case APP_AL_STATE_START:
    {
        if (AL_GetStatus() == SYS_STATUS_READY)
        {
            app_ALData.state = APP_AL_STATE_RUNNING;
        }

        break;
    }

Remarks

None.