5.2 Hardware Interface
This list shows the available hardware interfaces (Figure 5-1). If the user has more than one board with the Bluetooth Low Energy Sniffer firmware connected, the user can choose which one to control with the toolbar. For more details on using several hardware interfaces at the same time, refer to the Capturing from Multiple Hardware Interfaces.