5.5 Advertising Hop Sequence
In its default setting, the Bluetooth Low Energy Sniffer first waits for a packet on channel 37. After it receives a packet on this channel, it moves on to channel 38. After receiving a packet on channel 38, it shifts to channel 39. Upon receiving a packet on channel 39, it cycles back to channel 37 and the process repeats. The user has the option to customize the order that the Bluetooth Low Energy Sniffer switches between these advertising channels. The user can specify the preferred order by entering the channel numbers separated by commas. For example: 37,38,39. Press <Enter> to confirm the selection.