1.2.6.4.7 SRV_USI_Send_Message Function
C
size_t SRV_USI_Send_Message( SRV_USI_HANDLE handle,
SRV_USI_PROTOCOL_ID protocol, uint8_t *data, size_t length )Summary
Sends a message through serial interface (USI).
Description
This function is used to send a message through USI. The message will be formated depending on the specified Protocol and will be sent using the serial interface associated to the corresponding USI instance.
Precondition
SRV_USI_Open must have been called to obtain a valid opened service handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from SRV_USI_Open |
| protocol | Identifier of the protocol for the message to send (SRV_USI_PROTOCOL_ID Enum) |
| data | Pointer to the data to send |
| length | Length of the data to send in bytes |
Returns
Number of bytes sent.
Example
uint8_t pData[] = "Message to send through USI"; // 'handle', returned from SRV_USI_Open previously called SRV_USI_Send_Message(handle, SRV_USI_PROT_ID_PHY, pData, sizeof(pData));
Remarks
None.