SRV_PCOUP_Set_Config Function
C
bool SRV_PCOUP_Set_Config(DRV_HANDLE handle, uint8_t phyBand);Summary
Set the PLC PHY Coupling parameters for the G3-PLC PHY band.
Description
This function allows to set the PLC PHY Coupling parameters for the G3-PLC PHY band, using the PLC Driver PIB interface (DRV_PLC_PHY_PIBSet or DRV_G3_MACRT_PIBSet).
Precondition
The PLC driver's open routine (DRV_PLC_PHY_Open or DRV_G3_MACRT_Open) must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid instance handle, returned from the PLC driver's open routine |
| phyBand | G3-PLC PHY band for which for which the parameters will be set |
Returns
- true
- Successful configuration
- false
- if phyBand parameter is not valid
- if there is an error when using the PLC Driver PIB interface
Example
// 'handle', returned from DRV_PLC_PHY_Open or DRV_G3_MACRT_Open bool result; result = SRV_PCOUP_Set_Config(handle, G3_FCC);
Remarks
This function is only generated by MCC if the PLC Driver uses G3-PLC PHY.