1.1.1.4.6 DRV_PLC_PHY_PIBSet Function
C
void DRV_PLC_PHY_PIBSet (
const DRV_HANDLE handle,
DRV_PLC_PHY_PIB_OBJ *pibObj
);Summary
Allows a client to set information to PLC transceiver on PHY information base (PIB).
Description
This routine sets PHY data information to the PLC transceiver.
Precondition
DRV_PLC_PHY_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| pibObj | Pointer to the PIB object to set |
Returns
None.
Example
// 'handle', returned from DRV_PLC_PHY_Open previously called DRV_PLC_PHY_PIB_OBJ pibObj; uint8_t autoMode uint8_t impedance; // Disable AUTODETECT impedance mode autoMode = 0; // Set VLO impedance mode impedance = VLO_STATE; pibObj.pData = &autoMode; pibObj.length = 1; pibObj.id = PLC_ID_CFG_AUTODETECT_IMPEDANCE; DRV_PLC_PHY_PIBSet(handle, &pibObj); pibObj.pData = &impedance; pibObj.length = 1; pibObj.id = PLC_ID_CFG_IMPEDANCE; DRV_PLC_PHY_PIBSet(handle, &pibObj);
Remarks
None.