1.1.1.4.13 DRV_PLC_PHY_Tasks Function

C

void DRV_PLC_PHY_Tasks (
    SYS_MODULE_OBJ object
);

Summary

Maintains the driver's state machine.

Description

This function is used to maintain the driver's internal state machine.

Parameters

ParamDescription
objectObject handle for the specified driver instance (returned from DRV_PLC_PHY_Initialize).

Returns

None.

Example

SYS_MODULE_OBJ      object;     // Returned from DRV_PLC_PHY_Initialize

while (true)
{
    DRV_PLC_PHY_Tasks (object);

    // Do other tasks
}

Remarks

This function is normally not called directly by an application. It is called by the system's Tasks routine (SYS_Tasks).

This function will never block or access any resources that may cause it to block.