1.1.1.4.12 DRV_PLC_PHY_Status Function
C
SYS_STATUS DRV_PLC_PHY_Status (
const SYS_MODULE_INDEX index
);
Summary
Gets the current status of the PLC driver module.
Description
This routine provides the current status of the PLC driver module.
Precondition
DRV_PLC_PHY_Initialize should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| index | Identifier for the instance used to initialize driver. |
Returns
| Status | Description |
|---|---|
| SYS_STATUS_READY | Driver is ready to accept requests for new operations. |
| SYS_STATUS_UNINITIALIZED | Driver is not initialized. |
| SYS_STATUS_ERROR | Driver is not initialized correctly. |
| SYS_STATUS_BUSY | Driver is initializing. |
Example
SYS_STATUS status; // 'DRV_PLC_PHY_INDEX' is the one used before for Driver Initialization status = DRV_PLC_PHY_Status(DRV_PLC_PHY_INDEX);
Remarks
None.