1.2.1.3 Configuring the Library
PLC PHY Coupling Service can be configured through MCC.
Alternatively, the generated source/header files can be modified for custom configuration.
Configuring Through MCC
The following figures show the MCC configuration window for PLC PHY Coupling Service and brief description.
The configuration options will vary depending on the PLC protocol used by the PLC Driver (G3 or PRIME).
The configuration dynamic values (purple colour) will be updated, depending on PLC Driver mode and PLC Coupling settings in PLC Driver MCC configuration, in order to apply the configuration/calibration values for Evaluation Kits and/or reference designs.
G3 Configuration Options
- Transmission
Branches:
- Available only if G3 selected as PLC Profile in PLC PHY Driver MCC configuration, or G3 MAC RT Driver used
- Main Transmission
branch:
- PLC PHY Coupling configuration for Main Transmission branch
- Auxiliary
Transmission branch:
- PLC PHY Coupling configuration for Auxiliary Transmission branch
- Available only if Multiband enabled in PLC Driver MCC configuration
Each transmission branch is configured independently. In addition to Common Configuration Options, the following options are available for each transmission branch:
- G3-PLC PHY Band:
- Indicates the frequency band associated to the corresponding transmission branch, as selected in PLC Driver MCC configuration
- PLC DACC peripheral
settings:
- PLC Device's DACC peripheral register values (PHY PIB PLC_ID_DACC_TABLE_CFG)
- These values should not be modified by the user
PRIME Configuration Options
- Transmission
Channels:
- Available only if PRIME is selected as PLC Profile in PLC PHY Driver
- PLC DACC peripheral settings (Channel 1)
- PLC DACC peripheral settings (Channel 2 - Channel 8)
- PLC DACC peripheral
settings (Double Channel)
- PLC Device's DACC peripheral register values (PHY PIB PLC_ID_DACC_TABLE_CFG) for single channel 1 / single channels 2 to 8 / double channels
- These values should not be modified by the user
- Channel "i":
- PLC PHY Coupling configuration for single channel "i"
- Available
only if
Channel "i"is enabled in PLC PHY Driver MCC configuration
- Channels "i - j":
- PLC PHY Coupling configuration for double channel "i - j" (two consecutive channels)
- Available
only if
Channels "i - j"is enabled in PLC PHY Driver MCC configuration
Each channel is configured independently. Common Configuration Options are available for each enabled channel.
Common Configuration Options
- Number of TX
levels:
- PHY PIB: PLC_ID_NUM_TX_LEVELS
- Number of
transmission attenuation levels supporting dynamic capabilities
- G3: transmission attenuation levels in 3 dB steps
- PRIME: transmission attenuation levels in 1 dB steps
- Target RMS values in HIGH
mode for dynamic Tx gain:
- PHY PIB: PLC_ID_MAX_RMS_TABLE_HI
- RMS_HIGH_x:
- Target RMS values in HIGH Tx mode for transmission attenuation level "x"
- Target RMS values in VLOW
mode for dynamic Tx gain:
- PHY PIB: PLC_ID_MAX_RMS_TABLE_VLO
- RMS_VLOW_x:
- Target RMS values in VLOW Tx mode for transmission attenuation level "x"
- Threshold RMS values in
HIGH mode for dynamic Tx mode:
- PHY PIB: PLC_ID_THRESHOLDS_TABLE_HI
- THRESHOLD_HIGH_LOW_x:
- Threshold RMS values to update Tx mode from HIGH to LOW for transmission attenuation level "x"
- Set to 0 to disable
- THRESHOLD_HIGH_VLOW_x:
- Threshold values to update Tx mode from HIGH to VLOW for transmission attenuation level "x"
- Set to 0 to disable
- Threshold RMS values in
VLOW mode for dynamic Tx mode:
- PHY PIB: PLC_ID_THRESHOLDS_TABLE_VLO
- THRESHOLD_VLOW_LOW_x:
- Threshold values to update Tx mode from VLOW to LOW for transmission attenuation level "x"
- Set to 0 to disable
- THRESHOLD_VLOW_HIGH_x:
- Threshold values to update Tx mode from VLOW to HIGH for transmission attenuation level "x"
- Set to maximum value to disable
- Tx gain values for HIGH
mode:
- PHY PIB:
PLC_ID_GAIN_TABLE_HI
- GAIN_HIGH_INI
- GAIN_HIGH_MIN
- GAIN_HIGH_MAX
- Initial/minimum/maximum transmission digital gain value for HIGH Tx mode
- Set all to same value to disable dynamic Tx gain for HIGH Tx mode
- PHY PIB:
PLC_ID_GAIN_TABLE_HI
- Tx gain values for VLOW
mode:
- PHY PIB:
PLC_ID_GAIN_TABLE_VLO
- GAIN_VLOW_INI
- GAIN_VLOW_MIN
- GAIN_VLOW_MAX
- Initial/minimum/maximum transmission digital gain value for VLOW Tx mode
- Set all to same value to disable dynamic Tx gain for VLOW Tx mode
- PHY PIB:
PLC_ID_GAIN_TABLE_VLO
- PLC Line Driver
settings:
- PHY PIB: PLC_ID_IC_DRIVER_CFG
- PLC Device and branch
configuration. One value for PL360, three values for PL460:
- 0: PL360
- 5: PL460 using Main Transmission Branch with a single external filter. When transmitting, both ASO pins are activated simultaneously.
- 7: PL460 using Main Transmission Branch with two external filters. When transmitting, ASO0 is activated for HIGH Tx mode, while ASO1 is activated for LOW/VLOW Tx modes.
- 8: PL460 using Auxiliary Transmission branch
Modifying Generated Source Code
PLC PHY Coupling Service generates the srv_pcoup.c and
srv_pcoup.h files. In the header file there are definition
macros with the values configured through MCC.
The user can modify these files instead of using MCC interface.
In the current version, this is the only method to customize Tx Equalization values (not supported in MCC configuration window for PLC PHY Coupling Service).