SRV_PCOUP_Get_Channel_Config Function

C

SRV_PLC_PCOUP_CHANNEL_DATA * SRV_PCOUP_Get_Channel_Config(DRV_PLC_PHY_CHANNEL channel);

Summary

Get the PLC PHY Coupling parameters for the specified PRIME channel.

Description

This function allows to get the PLC PHY Coupling parameters for the specified PRIME channel. These parameters can be sent to the PLC device through PLC Driver PIB interface (DRV_PLC_PHY_PIBSet).

Precondition

None.

Example

SRV_PLC_PCOUP_CHANNEL_DATA *pCoupValues;

pCoupValues = SRV_PCOUP_Get_Channel_Config(SRV_PLC_PCOUP_MAIN_BRANCH);

Remarks

This function is only generated by MCC if the PLC driver uses PRIME PHY.

If SRV_PCOUP_Set_Channel_Config function is used to set the PLC PHY Coupling parameters, this function is not needed.