After generating the bitstream, the PolarFire device must be programmed with the system services design.
To program the PolarFire device, perform the following steps:
Ensure that the following jumper settings are set on the evaluation board.
Table 2-1. Jumper Settings for PolarFire Device Programming—Evaluation
Kit
Jumper
Description
J18, J19, J20, J21, and
J22
Close pin 2 and 3 for
programming the PolarFire FPGA through FTDI
J28
Close pin 1 and 2 for
programming through the on-boardFlashPro5
J4
Close pin 1 and 2 for
manual power switching using SW3
J12
Close pin 3 and 4 for 2.5
V
Connect the power supply cable to the connector J9 on Evaluation board.
Connect the USB cable from the host PC to the J5 on Evaluation board (FTDI port).
Power on the board using the slide switch SW3 on Evaluation board.
The following figure shows the board setup of evaluation kit.Figure 2-9. Board Setup—Evaluation Kit
The device is successfully programmed and the onboard LEDs 7, 8, 9, 10,
and 11 glow. A green tick mark appears next to Run PROGRAM Action.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.