1.1.33.1.7 WDRV_WINC_TLSCtxCACertFileSet
C
WDRV_WINC_STATUS WDRV_WINC_TLSCtxCACertFileSet
(
DRV_HANDLE handle,
WDRV_WINC_TLS_HANDLE tlsHandle,
const char *pCACertName,
bool peerAuth
)Description
Sets the certificate authority field of a TLS context.
Precondition
WDRV_WINC_Initialize must have been called.
WDRV_WINC_Open must have been called to obtain a valid handle.
WDRV_WINC_TLSCtxOpen must have been called to obtain a valid TLS handle.
Parameters
| Parameters | Description |
|---|---|
| handle | Client handle obtained by a call to WDRV_WINC_Open. |
| tlsHandle | TLS handle obtained by a call to WDRV_WINC_TLSCtxOpen. |
| pCACertName | Pointer to certificate authority name. |
| peerAuth | Flag indicating if peer authentication is enabled. |
Returns
- WDRV_WINC_STATUS_OK - The request has been accepted.
- WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open.
- WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
- WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
Remarks
To ensure proper authentication checks are performed the value of peerAuth should always be 'true', setting this parameter to 'false' will weaken authentication checks.