Framed SPI Errors
If the transmit buffer is empty when the SPI must load the shift register to start (in the case of Framed Client) or continue (for either Framed Host or Client) a transfer, the SPI immediately sets the transmit underrun status bit in the STATUS (STATUS.TUR) register. If enabled, an Error interrupt flag (INTFLAG.ERROR) will also be generated.
While the SPI is in an underrun condition, the SPI transmits all zeroes until the end of the transaction (byte, word or length counter). If the SPI is a frame client, another frame sync pulse can occur before the condition clears. In this case the SPI continues to transmit zeros. If the SPI is a frame host, it then waits for software to clear the under-run condition before initiating another FSYNC regardless of the state of the DATA buffer.
When the TUR status is cleared the data present in the DATA buffer is flushed. The SPI ignores writes to the DATA after clearing the STATUS.TUR bit, until a read of STATUS register, when STATUS.TUR=0. This behavior ensures that a data service routine that is interrupted long enough to cause STATUS.TUR, cannot inadvertently start a new framed transaction after the SPI error handler has cleared the error.
For cases when software does not care or need to know about the underrun condition, CTRLC.IGNTUR = 1 provides the serial engine the ability to ignore the underrun. When an underrun occurs, the SPI still sets the corresponding STATUS and INTFLAG bits. When the SPI is either a frame client or a frame host, an underrun event still causes the SPI to transmit zeros until the end of the frame. However, when the Ignore Transmit Underrun bit is set (CTRLC.IGNTUR = 1), the SPI can re-sample the underrun condition and continue to transmit data at each frame boundary. If the SPI is a frame host, new data written to the DATA buffer during a frame when an underrun condition exists does not get transmitted during that frame. But, the SPI evaluates the DATA buffer continuously after the last frame. If data is in it, the SPI generates a frame sync and transmits the data. If the SPI is a frame client, its transmit logic evaluates DATA buffer for underrun during the next FSYNC. If the buffer contains data when a valid FSYNC is detected, SPI transmits that data. If not, the SPI transmits zero data until the end of the frame.
In the case of client frames, if a new FSYNC is received during an ongoing frame transaction, the transaction length error status bit is set, and the error interrupt flag is set. The module will continue to send data from the internal buffer.