16.5.4 Configuration Flash Memory Layout
The Boot ROM utilizes a predefined Configuration Fuse Memory (CFM) layout to manage boot-time settings. This layout includes dual copies of the boot configuration, providing redundancy to enhance reliability.
The Boot ROM attempts to boot the device as long as at least one of the BOOTCFG memory regions is valid and passes integrity checks. However, it is strongly recommended that both BOOTCFG fuse regions be programmed to take full advantage of the available redundancy and ensure robust boot behavior.
Device USERCFG 1/1A and ROMCFG Fuses
The Boot ROM supports complete device configuration through the User Configuration Fuses (USERCFG1/1A). To enhance reliability of the device, the Boot ROM maintains two physical copies of the user configuration:
- USERCFG1
- USERCFG1A
The Boot ROM selects one of these fuse sets during the boot process, selected by configuring the SEQ and SEQBAR fuses. If both USERCFG1 and USERCFG1A fail integrity checks, the Boot ROM halts the boot process and places the device into interactive mode.
Selection of USERCFG1 v/s USERCFG1A
The Boot ROM uses Firmware Metadata (FWMD) provided by the user to determine which boot configuration to use. This metadata includes two 32-bit unsigned integers:
- SEQ0: Associated with USERCFG1
- SEQ1: Associated with USERCFG1A
These sequence values are used to determine which configuration is more recent or preferred.
The Boot ROM selects the boot configuration based on the following conditions:
| Condition | Selected USERCFG fuse for Boot |
|---|---|
| SEQ0 > SEQ1 | USERCFG1 |
| SEQ1 > SEQ0 | USERCFG1A |
| SEQ0 = SEQ1 and both ≠ 0xFFFFFFFF | Boot Process halted, Boot ROM goes to Interactive mode |
| SEQ0 = SEQ1 = 0xFFFFFFFF | Boots using default USERCFG values |
Device ROMCFG Fuses
The ROMCFG region contains critical fuses that allow users to configure device access, enable self-tests, and enforce security policies. These fuses are evaluated by the Boot ROM during the early boot phase. Below is a summary of the key fuses within the ROMCFG region.
DAL Fuse
This fuse determines the Debugger Access Level (DAL) that becomes effective after the Boot ROM completes its execution and transfers control to the user application.
- DAL2: Full access (value = 0xFFFFFF55)
- DAL0: Locked state (any value other than 0xFFFFFF55)
FRCFGBROM Fuse
This fuse enables an internal self-test of the Boot ROM memory contents. If enabled and the self-test fails, the device halts further execution.
- Default State: Disabled after any reset
- User Action: Must be explicitly enabled via fuse programming
FRCFGMBIST Fuse
This fuse enables Memory Built-In Self-Test (MBIST) on the entire device SRAM. If MBIST is enabled (e.g., MOBB = 0x1 or 0x2), the Boot ROM checks the MBIST result during boot.
- If MBIST Fails: The Boot ROM halts the boot process and enters an infinite loop followed by a software reset.
- If MBIST Passes: Boot continues normally.
KEYVAL_ Fuses
The ROMCFG region includes multiple KEYVAL_ fuses used for device-specific configuration and security enforcement.