8.3.9 L: Library Path Option
The -L dir option or
its alias --library-path dir adds dir to search path the linker will use to find
libraries.
This option adds path dir to the list of
paths that xc32-ld will search for archive libraries and
xc32-ld control scripts. You may use this option any
number of times. The directories are searched in the order in which they are specified on
the command line. All -L options apply to all libraries
specified using -l options, regardless of the order in
which the options appear. The library paths can also be specified in a link script with the
SEARCH_DIR command. Directories specified this way are
searched at the point in which the linker script appears in the command line.